Basic Freq & Phase Error

Limits

Check the Tolerance Limit box to set a pass/fail limit for the frequency error result, and enter the value in parts per million.

Settings

Enter a value for Digital IF BW in MHz, to manually set the digital IF bandwidth of the receiver path for basic frequency error measurement when None is selected as the radio standard for the acquisition. This is used to set the hardware of the digital receiver.